Other Parts Discussed in Thread: BQ25731, , , TPS25751, BQ25713
Hi,
I have been trying to find an answer to this issue for nearly a month with no results. I am using a custom circuit board which is basically identical to the TPS25750EVM board (TPS25750 + BQ25731 + EEPROM). When I generate the configuration file for both source and sink and upload it to the EEPROM and restart the devices (power reset), I see that the EEPROM is read. But when I connect a USB-C cable so that I charge a device for voltages larger than 5V, I see the TPS25750 trying to access register addresses of the BQ25731 which do not exist, causing either the TPS25750 or the BQ25731 to keep the I2C clock line low. The following thread had the same issue and Alex Liu provided a bin file that worked for sourcing power. The issue is that not all setting are as I wish them to be.
Is there planned any solution to solve this bug? We are in the need to solve this issue urgently as we need to finalize the design to start production. If its is not solved quickly, we would have to change the design and find other devices.