This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ35100: EOS bit

Part Number: BQ35100
Other Parts Discussed in Thread: BQSTUDIO

Thank you for the log file.

More information is required from you before I can help you.

 ################################################

Please share a bqstudio log file of the EOS bit not functioning as expected.

Please provide more information about the system what type of battery is the customer using?

What is the pack configuration?

When does the customer expect the EOS bit to flip?

You mentioned the voltage drops to 0V, can you further explain this?

You said you have not programmed the chemistry because it is not required for eos mode, what do you mean by this?

 

Can you additionally share the .srec file so I may view private parameters.

Regards,

Fabio