This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5157: Vout:30V; Iout:6A condition

Part Number: LM5157

Hi Team,

My requirement is that the input voltage is 16V and needs to be converted into an output voltage of 30V/6A. Have any suggestions?

  • Hi Kevin,

    Thanks for using the e2e forum.

    For a boost design with 180W output power, I would recommend a synchronous Boost controller, which uses a high side switch instead of a diode to increase efficiency at higher load.
    A suitable part for this would be LM5123.
    You can take a look at the EVM board for reference, which is design for similar specs but lower output power.
    https://www.ti.com/tool/LM5123EVM-BST

    Please let me know if you have additional question on this device.

    Best regards,
    Niklas