This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2373-4EVM-758: Combination of evaluation boards to meet required specifications

Part Number: TPS2373-4EVM-758
Other Parts Discussed in Thread: TPS2373, , PMP20878, PMP

Hi,

The customer would like to achieve the following specifications:

・PoE++ (IEEE 802.2bt)

・PD

・Type 4

・Class 8

・Output Voltage=24V

Is there an evaluation board that can be used in combination with TPS2373-4EVM-758 to meet the specifications? Since TPS2373 is an interface, I am looking for an evaluation board for the power part.

There are materials for PMP20878, but the design takes time, so I would be happy if it could be realized with an evaluation board.

https://www.ti.com/tool/ja-jp/PMP20878#tech-docs

Best Regards,

Nishie