Hi there,
Our application requires ideal-diode ORing only, no hot swap function.
We have two same 12V battery packs and want to do power ORing of their outputs.
Estimated maximum load current is around 15A.
The battery pack does not allow direct parallel connection.
So my plan now is as follows,
1) No hot swap NMOSFET's
2) Connect downstream side of two Rsens's together. Connected line goes to load.
3) Connect ENHS to GND
4) Leave OUTH, HGATE pads floating
I know that there is more simple solution using other IC,
but I want to do current monitoring for both battery packs so I picked this IC.
Please let me know if this plan works.
Toru