This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25927: About output capacitor recommend condition

Part Number: TPS25927


Hi team,

Our customer want to use this device to below condition,

 Vin:15V

 Iload:max1A

 Output capacitance:6000uF

 Cdvdt=0.047uF

In this condition, Tdtdv = about 700msec. So the power dissipation by inrush current is 956mW. So in this power dissipation, Tdvdt is below thermal shutdown time @Ta=25C.

And Junction-to-ambient thermal resistance is 45.9 C/W. The thermal increase is about 43.9C. 

So I think we can use this device in this condition. But the recommend condition is max Cout is 1000uF.

Could you please give me your opinion on the above?

Best regards,

teritama