This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: Reading FW Version

Part Number: BQ76952

When reading the FW version in the bq76952 using subcommand 0x0002, the TRM indicates there are 6 Bytes of data to read back.  But checking the data length using Command 0x61 indicates the data length is 11. Datalength read back 0x61 returns 0x0F (15 dec). Subtract 4 bytes and result is 11.  

When we read the 11 bytes, only the first 6 have data, the last 5 bytes are all 0x00. 

Is this correct?