We wish operate the at 48VDC input to the final drivers and output 36V pulses at 45% duty cycle at minimum of 4 amps per pulse output into a toroidal HF planar transformer. We noticed that the efficiency is not good at these levels. Are we missing something. Is there an alternative TI GaN driver?
We plan to use two units as a push-pull H bridge combination to create the 36-42 Volt pulse out at the pulse current of 4 amperes.
We are seeking at least 95% at the stated levels output to the transformer as intimated above. Is this feasible?