Hi,
I want to use your UC3625 motor control IC to excite 6 isolated IGBT driver and eventually to drive High Voltage IGBTs.
IGBT specs may be : IC25 = 225 A VCES = 600 V VCE(sat) typ.= 2.0 V
IGBT Isolated Driver ACPL 332J
Motor will be a high voltage one, not certain but it will be over 300V 15Amps
Could you provide me a design note which includes your motor controller UC3625 ? I've already checked your ANs on the product page but they do not enclose a general design. Maybe if you have a sketch up with fet or igbt drivers and hall sensors tied together.
Thank you for your time.