This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62932: Frequency setting

Part Number: TPS62932

① the switching frequency when I exit PFM mode is different from the set frequency.
When the load is low even after exiting the PFM mode, does the set frequency sometimes not reach?

② the frequency setting is set to 2.2MHz, but the setting may be 2.2MHz or higher due to the variation of the resistor.
Is there any problem as a DCDC even if it is set at 2.2MHz or higher?