Hi Team,
Could you tell me recommended resistor value of pull-up/pull-down for MODE-pin?
When logic is high it works in forced PWM, when logic is low it works in auto PFM.
Best Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Could you tell me recommended resistor value of pull-up/pull-down for MODE-pin?
When logic is high it works in forced PWM, when logic is low it works in auto PFM.
Best Regards,
Hi Atsushi,
It is ok to add pull-up/pull-down resistor between signal and MODE, but it is not recommended to use >1M ohm as this would introduce noise to MODE pin.
Regards,
Nathan
Hi Nathan-san,
Thank you for your reply.
What method should user generally use to fix the logic(High or Low) of MODE-pin?
Please let me know if there is a recommended method than pull-up/pull-down.
Hi Atsushi,
Usually we connect MODE with GND or VIN to fix the logic low or high. You can refer to the schematic in EVM user guide.
Of course other general pull-up or pull-down ways are ok. There isn’t any special requirement except the resistance I mentioned above.
Regards,
Nathan