This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5176: The LM5176 inductance is hot

Part Number: LM5176
Other Parts Discussed in Thread: LM5175

Hello, I have a project using LM5176. The input voltage is 11V-25V, the output is 12V, the switching frequency is set to 100KHZ, the subsampling resistance is 3mΩ, the output sampling resistance is 3mΩ, the conversion inductance is 3uH, and the DC impedance of the inductance is 3mΩ. It is found that the temperature of the inductance is about 50-60℃ when the inductance is unloaded. I would like to ask how to improve the temperature of the inductor and output capacitor.