Hello,
I am working on a battery management system and have zeroed in the BQ76942 as the core IC with a setup similar to the datasheets recommended configuration, with the REG voltage outputs supplying current to the auxiliary components, but their max current draw is 45mA.
The communication transceiver would be a 5V CAN bus transceiver, yet I could only find ones that required about 70mA in dominant mode.
Is there a recommended CAN transceiver chip for a system which uses the BQ76942 ?
thank your time and help !