This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: SUV

Part Number: BQ40Z50-R1
Other Parts Discussed in Thread: BQ40Z50, BQSTUDIO

If I want to enable the SUV function in PF, the FUSE pin grounding of the BQ40Z50 chip is not used, and only Settings:Enabled PFA in the upper computer of BQStudio is set, the SUV is set to 1 and the SUV threshold is set to 2000mV. Do you need to configure anything else? Why does the FET not turn off when the cell voltage reaches below 2V?

  • Hello,

    Is it possible to send a .gg file of the gauge settings and a log file of SUV attempting to be triggered by the gauge? This will allow us to pin point the reason the SUV protection is not triggering.

    Regards,

    Anthony Baldino