Other Parts Discussed in Thread: TPS563252
Hello,
TI part PTN4050AAZ is obsolete. We have several products with it we need to support. I need to design a DC-DC as an inverter in the same footprint as a tiny daughter card so I can replace PTN4050 with the newely designed DC-DC in my PCB
Can you help me find an inverting DC-DC? I have two configurations to support. 5V IN to -6V (At 1A max) or 5V (At 1A Max).
It looks like TPS62913 can be set up for Inverting buck boost (IBB)?
Is there are newer part? If so can you help me design a circuit for achieving the same functionality as PTN4050AAZ?
Also, there are 5 pins on the PTN4050AAZ. Can you tell me what that part number is I can incorporate the same on the PCB I am designing.
Thanks,