Hi!
If I am reading the datasheet (section 6.4.1) and related questions correctly, the DEMB resistor sets the load current at which the low-side fet switches from diode to synchronous mode?
"When RDEMB=0, the LM5116 will always run in diode emulation."
and
"Full synchronous operation is obtained if the DEMB pin is always biased to a higher potential than the SW pin when LO is high. RDEMB = 10 kΩ will bias the DEMB pin to 0.45V minimum, which is adequate for most applications"
However, I haven't been able to force the low-side fet to stay as a diode or synchronous mode no matter what resistor I populate for RDEMB. The traces below show load current (yellow, with "value" measurement), low-side fet gate voltage (magenta) and switching node voltage (cyan). According to the datasheet, the plots should be the same for the resistor values I used here, but this is not the case.
One minor notice is that it takes a much higher current for the 0ohm circuit to enter synch mode and vice versa at least, so I'm assuming something is working.
| low current (diode mode) | in between (sometimes diode or synch mode) | high current (synch mode) | |
| 0 ohm RDEMB (should theoretically only ever be in diode mode) | ![]() |
![]() |
![]() |
|
open circuit RDEMB (should theoretically always be in synchronous mode) |
![]() |
![]() |
![]() |