Other Parts Discussed in Thread: TPS552882
Hi Support team,
I want to use TPS552892 in my design, the System requirements are:
Vin range = 3-20V, Max Iout = 3A and need to have both Vout = 5V and Vout = 12
I have concern at low input voltage, Vin= 3V, Dose the part can provide 3A output current for Vout = 5V and 1.5A for Vout = 12 ?
Also I don't have external 5V available, Do I just connect Vcc to EXTVCC? Is this case still work for low input voltage Vin= 3
If I need to useTI Pspice model do I need to purchase the software?