This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8758-EA: The Vout step size range

Part Number: LP8758-EA


Hi,

PMIC LP8758-EA Vout programmable voltage range Step size between 0.73 V ≤ VOUT < 1.4 V is 5mV, we need to Vout 0.6V/ 1.1V/ 1.8V step size less than 3mV, so is there any promoted? thanks.