This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25628: Output is at 1.0V

Part Number: BQ25628

When 12V power is applied to the BQ25628 on my PCB, the output is a solid 1.0V instead of the 3.75 I was expecting. I cannot find anything about 1.0V in the datasheet. Charging is disabled by default in my design and there is currently no battery hooked up. Also, the chip has not been programmed. Nevertheless, as I understand the datasheet the output voltage should still be above VSYSMIN which is 3.52V per the datasheet. Schematic is shown below.