Other Parts Discussed in Thread: TPS923654, TPS923655
The TPS923653DYYREVM is originally configured for boost mode.
Boost Mode Sanity Check:
I'm testing with a ~26V LED load. When input voltage is near 26V, input current is a little over 2A. Seems right for output 2A and Vout ~= Vin.
When I decrease input voltage, the input current goes up. OK, normal boost behavior.
Configuring for Boost-Buck Mode:
I disconnected LED minus from GND and connected to Vin. This configures buck-boost topology.
I decreased the value of R6 to 31.3k. So I'm expecting overvoltage protect at theoretical 52.7V (Vin + V_LED).
I apply input voltage. Works with no fault between 11V ... 27.5V.
11V fault is maybe FET overcurrent, ok. 27.5V fault is probably OVP (Vin + V_LED), ok.
But in this ok voltage region, indicating no fault, the input current is low. At Vin = 26V the input current is 1.16A. It should be above 2A.
I haven't put a meter in the output yet, but obviously it is lower than the 2A output current EVM set point which worked correctly in boost mode.
Is there some other change required to configure buck-boost mode on this EVM? Thank you.