This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello TI team,
I have query regarding the MPPT setting in BQ24650. As looking in datasheet it provides two types MPPT setting as per below image. Please refer page no 23 and 27 in datasheet.
Method 1 Method2
Please look it here and suggest further.
Regards
Paresh Panchal
Hello Paresh,
Is your design going to support a solar power input?
Best Regards,
Christian.
Hello Christian,
Thanks for revert, Yes, my design is support the solar power input.
Hello Paresh,
From above which one method is good ?
They serve different purposes.
The LMP234 is used to compensate the negative temperature coefficient of the solar panel output voltage as per the section 9.2.2.6 MPPT Temperature Compensation of the datasheet.
The MOSFET is used for enabling and disabling charging.
I recommed refering to this app note: https://www.ti.com/lit/an/slua586a/slua586a.pdf
Best Regards,
Christian.