I have used TPS55289 to design a buck boost with VIN 8V to 24V and Vout set to 14V, i am not using any I2C as i assume it is just to read the data and TPS55289 IC is stand alone IC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have used TPS55289 to design a buck boost with VIN 8V to 24V and Vout set to 14V, i am not using any I2C as i assume it is just to read the data and TPS55289 IC is stand alone IC
Hello Brigitte,
Could you please confirm the data and addresses I selected as per my requirement
Requirements
Mode pin set to LOW
Output feedback set to external
- Feedback calculated considering Vref = 1.129V
Output current limit is disabled
Address - 75h
DATA - HEX Value 28,05, 64, 01, 83, E7, A2, 00
Hi Rahul,
When the value of 0x00 and 0x01 is 28, 05, the reference voltage is 790.14mV, rather than 1.129V.
And with below register value, you can set Vref=1128.84mV.
BRs,
Bryce
Hi Rahul,
This is the GUI software where you can download from the below link at the EVM User Guide.
https://dev.ti.com/gallery/info/TPS55289/TPS55289/
BRs,
Bryce