This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21520: UCC21550BQDWRQ1 OUTA not switching

Part Number: UCC21520

Hi,

I have  UCC21550BQDWRQ1 circuit, which is attached. The PWM controller is UCC28086D at 33kHz. The input works fine. Concerning the output, only the OUT B is switching ON/OFF but the OUTA goes high and reads 10V, i.e., stays ON without switching.

I have supplied the isolated rail with 11.5V, both VDDA and VDDB share the same power rail. In the previous question awhile ago, I was told that both can share the same PSU. 

What could be the issue?

Kind regards,

Bright

Isolated Dual-Channel Gate Driver.pdf