Hello experts,
I am a bit confused about TLV76780 operation,
for all of the packages we have several different nominal Vout devices, like for HVSSOP, we have 25 for 2.5V, 28 for 2.8V, etc.
However for DBV package we only have 80, which I assumed meant 8.0V, but max Vout value is 6.6V for TLV767 family.
What is the vout operation range for TLV76780, and how does customer adjust the operating vout? Customer has 12V -> 5V power rail.
Also, in comparison, how does TLV76750 work? What is the vout operation range for TLV76750, and how does customer adjust the operating vout?
I hope to compare the two to the customer, but I couldnt find any comparison table on the datasheet, except that the packages are different.
Thank you.