Hi Team,
We are observing an issue with the TPS259461L.
We are using it as switch for controlling output power to a daughter board.
The setup:
Input power is derived from a DC power supply - set at 7.4V with 10A limit.
The output power is connected to a DC programmable load - set at CC of 5A, and being turned on/off manually.
The control of the eFuse is from a microcontroller (which drives the EN/UVLO high/low, and an external 100K PD is also attached to the pin)
Additionally, there is a 7.5K PD on the OVLO pin.
What we are observing is that when we turn on the eFuse, and then load it with 5A, and then subsequently turn it off, the output remains conductive.
The EN/UVLO pin and OVLO are both low.
Toggling the EN/UVLO pin has no effect, however tripping over-current or driving OVLP pin high causes the eFuse to switch off as expected.
We cannot figure out why the eFuse won't swtich off when EN/UVLO is driven low.
Any help on this matter would be appreciated.
Kind Regards