This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: ALERT PIN / Alarm Status

Part Number: BQ76952

Hi

I use ALERT PIN for safety alert.
For example, when a COV occurs,  I  confirmed that the COV of SafetyStausA (0x03) is 1, the SSA of AlarmStatus is 1, and the ALERT PIN changes from low to high.
When COV is released, the COV of SafetyStausA (0x03) is 0, but AlarmStatus and ALERT PIN remain the same.
I wrote 0xFFFF to AlarmStatus, but AlarmStatus and ALERT PIN remain unchanged.

Is there a way to reset AlarmStatus and ALERT PIN?

I want to detect the re-occurrence of a safety alert by the edge of the ALERT PIN as well.

Thanks with Regards.