Hi,
I am using the LMQ61460AASRJRR for a high current DCDC convertor. Input is 14V to 28V, and output is 12.1V at 4A. It is powering either a load circuit (a resonant LRC circuit being switched on and off at 3kHz by a half-bridge, which will draw 2A rms) or two generic resistive loads (of upto 2A rms each). The schematic is literally identical, and the layout is very nearly identical to the eval board, which is also showing the same problem.
We are seeing large over- and under-shoots on the switch node. The worst is by far the negative going edge on the switch node, with a lot of settling ripple, and this is causing 60MHz noise problems.
I see from the other post on this issue (e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/980090/lmq61460-excessive-ripple-and-dropout-spikes-with-load-current-of-3-5a-or-greater?tisearch=e2e-quicksearch&keymatch=LMQ61460AASRJRR) that someone else had a similar problem but the solution wasn't shared with the community.
We have tried multiple things - increasing the turn-on time sorted the overshoots but the undershoots can't be slowed down, a Schottky diode from ground to the switch node to clamp the undershoot, changing the switching frequency, etc.
Can you advise further?
Many thanks,
Murdo.