Other Parts Discussed in Thread: LMR38020
Hi,
I have a board with the attached schematic for an LMR38020-Q1. This DC/DC converter gets its power from the same rail which has a large 48V compressor which we PWM for a few milliseconds as a means to soft start the compressor in order to extend the compressors life. During this PWM phase there is a large amount of voltage ripple (20V -30V) on top of the 48V battery voltage. This ripple sometimes falls below the falling level of the converters under voltage lockout, Sometimes the under voltage lockout trips and causes the 24V rail to fall to zero and other times it does not. I have also observed 2 of the boards fail in a way that the DC/DC converter burns off its case. This is leading me to believe there is something causing the converter to experience a shoot through event. Is it possible that the logic inside the DC/DC converter somehow gets confused and turns on both the low and high side mosfets?