This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: BQ7695202

Part Number: BQ76952

Hi TI Team,

                    Currently i am using BQ7695202 for our BMS application. I am facing a issue of I2C communication break between BQ7695202 BMS IC & host microcontroller when we set the cell balancing of 9 cells. When start balancing of 1 cell then near about 70mA current is flow. When we set the cell balancing of 8 cells then no I2C communication break. But when we set the cell balancing of 9 or more cells then BQ7695202 IC break the I2C commuication with host microcontroller. At this time BQ7695202 IC temperature is 37 degree celcius. We don,t know why this is happening. 

Please help us to resolve this issue.

Thanks with Regards,

DEEPAK