Other Parts Discussed in Thread: TPS92201AEVM, TPS92201
Hi Sir,
My customer is using the TPS92513 for the IR LED applications.
They found when PDIM = 0V, still can see the weak IR light on the lens.
In the same time, they found the PH pin still has 1.8V, they also try to remove the IR LED, the PH pin will rise to 3.3V.
Is this normal? How to trun off the weak IR light?
BTW, they also try to adjust the PWM frequency down to 100Hz to 1kHz, still can see the weak IR light on the lens. Even do the same test conditions on the TPS92513EVM, also got the same results.