This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] BQ2575X: Input And Output Capacitors

Part Number: BQ25756

Hello,

For the BQ2575X family, 80µF is the minimum after derating for the input and output capacitance. 160µF of input and output capacitance is based on meeting a ±3% transient response requirement.

Keep in mind, you'll also need to balance the capacitors across the RBAT_SNS and RAC_SNS resistors. It doesn’t need to be 1:1 across the resistor. You'll also need a small MLCC decoupling cap close to the switching FETs for both the input and output. A 1µF cap should work here. This cap will help filter out high frequency noise from the switching converter. The picture below shows how the electrolytic capacitors and ceramic capacitors are placed across the current sense resistors.



This advice will apply to all parts in the BQ2575X and BQ2585X family.

Best Regards,
Ethan Galloway