This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV810E: Suitable reset supervisor for SSD1315

Part Number: TLV810E
Other Parts Discussed in Thread: TPS3422, TLV803E

Hi all. This is the required reset waveform for an OLED controller I am using (SSD1315):

https://cursedhardware.github.io/epd-driver-ic/SSD1315.pdf (page 24)

At first glance the TLV810E seemed suitable because it has a built-in delay. However, after this delay it only goes LOW, while I need it to generate a pulse (go HIGH again).

Could I still use this chip to achieve this functionallity with some additional circuitry?

Or is another chip required? If so, which type?