This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ35100: how to properly configure GNDSEL

Part Number: BQ35100

Dears,

BQ35100 is configured in EOS mode ,

VSS pin is connected to the system ground,

SRN pin is connected to the system ground through 100 ohm (filter resistor) as in the evaluation board.

  1. is it ok to set ADC ground 0 (SRP is ADC GND) or it should be 1?
  2. how the wrong selection would affect the measuring, and should the calibration be redone?

Kind regards