Hi team,
My customer wants to use TPS92643-Q1 for a constant current drive design of the solenoid valve and has the following questions:
1. High side short circuit to power +12V/ground (below LED+), short circuit capability is 100A-max, can the upper and lower MOS inside the chip withstand this type of test?
2. The actual current of the load can be read by the MCU?
Thanks!
Regards,
Ivy