This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A88-Q1: Single output using both channels

Part Number: TPS7A88-Q1


Hello,

Is there a recommendation on combining both output channels as a single output? The way I see it is that the outputs could be combined before the voltage divider and output filtering, which would allow a single set of passive components and both output channels would utilize the same voltage divider as feedback. This should allow both outputs to be relatively close or almost identical to each other. My worry is that if there are two separate outputs with two sets of passive output components, then when combined after the output filtering, they may be slightly different to each other. Would that cause issues with the device?