Hi all,
I need to do a design with those specs:
Vin: 48Vdc
Vo:400Vdc
Io:.0.5 Amps
I don't know which could be the best topology, nor the IC, any suggestion will be highly appreciated!
Thanks and regards,
Xavi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I need to do a design with those specs:
Vin: 48Vdc
Vo:400Vdc
Io:.0.5 Amps
I don't know which could be the best topology, nor the IC, any suggestion will be highly appreciated!
Thanks and regards,
Xavi
Hi Xavier,
I see that this is listed under isolated supplies.Do you absolutely have to have the input isolated from the output?
I ask this because the solution for a non-isolated solution is trivial in comparison with an isolated solution.
Please respond to this and we can take it from there. Neil F. Pattison.
Hi Neil,
Actually it's not necessary, I firstly posted this message to the non-isolatde, but it was moved to here.
Is there any solution for non-isolated at 400V?
Regards,
Xavi
Hi Xavier,
One non-isolated solution is to use a "LINEAR TECHNOLOGY" LTC3862-1 polyphase boost controller feeding a pair of 600 volt fets with 600 volt SiC diodes isolating the 400 volt output.This is what I would use if I needed to implement your requirement.Their datasheet shows a suitable circuit,you will just have to modify a few components.I can offer further assistance if you need it.
Unfortunately,TI do not appear to have a suitable polyphase boost controller which will do the job.
Regards, Neil F. Pattison.