This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Expert,
My customer application is input:8-32V, charge Voltage:12.6V charge Current:5A.
The customer hopes that a short battery will not cause system shutdown and can continue to power the system.
I did not see any more information about battery short in the datasheet. Can you help me verify it?
In addition, if there is no battery, can the system provide VSYS voltage normally?
Thank you.
Darren
The system should work normally if there is no battery but the system will not work if the battery is shorted because the system power comes from the BAT.
Hi Utasv,
The customer hopes that a short battery will not cause system shutdown and can continue to power the system.
Do we have the solution for this? How about use BQ25750 with power path?
Thank you.
Darren
Hi Darren, I don't think there is a solution for this. The system was designed in a way to shutoff the system in case of the shorted battery to protect the system.