Other Parts Discussed in Thread: BQ25620
Dear TI experts,
My customer is lookng for the charger IC which meets the conditions below;
1. The battery is Li-ploymer, 1-cell, 4000mAh,
2. Charging current : 3A
3. Have internal power path.
4. have shipping mode, and can wake up from shipping mode using dedicated pin. (customer will connect tact switch to the pin.)
- The customer wants no current through power path during shipping mode, so main MCU cannot operate.
5. Standalone control interface is preferred.
Please check this issue. Thanks.
Best regards,
Chase