This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2803: perennity confirmation

Part Number: UCC2803
Other Parts Discussed in Thread: UC2843A

Hi,

I'm considering UCC2803 to implement a flyback converter on a new design for which i need 8-10 years perennity.

I have seen that this part is around since 1999, just want to make sure that TI does still recommend it

for new designs and will continue to support it, as it looks pretty unique regarding the input voltage.

UC2843A looks more generic but I have to manage a 7VDC min input voltage...

Thanks

Regards

Julien