This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7310: Problems importing LM73100 Pspice model to LTspice

Part Number: LM7310


I am trying to import the LM73100 Pspice model into LTspice using the same method as I have with other components. When I try to run the simulation I get an error saying "unknown spice device type "1" in ..."

When I open the .lib file I see that the component information appears encrypted, whereas usually it is written in a manner that is understandable to humans. I wonder if this encrypted component information is causing problems in the LTspice.