UC3825 dead time is the dead time of the oscillation frequency? UC3825 finally outputs two paths, and the dead zone time of these two paths is 1/2? The dead zone of the oscillator if nothing else is considered, is the dead zone time of the output pwm 1/2 related to this?