Part Number: BQ28Z610
Other Parts Discussed in Thread: BQSTUDIO
Hi,
i have a problem with the charge abilitation:
I'm using the bq on voltage thresholds instead of SOC% for protections ecc...
My device is connected to the charger and it's at 100%.
After some days my battery drop to 92% with a voltage level of 8170 mV (with both registers TC and FC CLEAR voltage at 8200 while the registers are SET at 8400) but nothing happen while still connected to the charger.
these are the values of the registers while at 92% and still plugged in the charger: DSG = 1, CHG = 1, XCHG = 0 and XDSG = 0 (so the charge is enabled since i'm under the clear voltage of 8200 mV and without faults).
But the charge starts only if i disconnect and re-connect the charger on the device.
What can i do in order to let it charge without the "reset" with the disconnection of the charger?