This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27426: BQ27426

Part Number: BQ27426
Other Parts Discussed in Thread: GPCCHEM

Hi All,

I am working on BQ27426 fuel gauge. I wanted to know the answer of few questions

1. I have configured the fuel gauge with the golden learning data

2. I have also configured the battery chem ID to 3142

But still I am not getting the accurate readings of the battery, I can see there is an offset in the battery voltage.

Golden learning data was performed on a 530mAh battery and I am working on a different battery (410mAh), 

Could that be the reason for inaccurate readings?

is there anything else to be configured so that I get the accurate values from the fuel gauge?

Any help is appreciated

Thanks

  • Hi Aldrina,

    For clarification, after completing the golden learning with a 530mAh cell, a 410mAh cell has been attached to the gauge?

    If so, this is most likely the issue. Changing the cell after golden learning has been done on a different cell will greatly effect the performance of the gauge since the values and measurements taken are for a different cell.

    If you are using the 410mAh cell, we would recommend completing another learning cycle with that cell attached.

    Regards,

    Anthony Baldino

  • Hi Anthony

    Thanks for the reply and suggestion I will check that. I wanted to confirm , what else needs to configured other that the golden learning parameters and configuring the chemID to get accurate values. As of my knowledge the BQ27426 is a ROM based gauge and we can configure only three custom chemID's right? Are there any more configurations to be done to get accurate values?

    Thanks in advance

  • Hi Aldrina,

    Yes, for bq27426 there are only 3 configurable chemIDs that can be used. We would recommend using the GPCCHEM tool to find the best fit.

    Before learning, the most important parameters to configure are the golden learning parameters such as Design Capacity, Term Voltage, etc. After the learning cycle is done, it is much easier to tweak the other parameters to fit the application as seen fit. If there are accuracy errors that occur after the learning cycle, please let us know and we can work through them.

    Regards,

    Anthony Baldino

  • Hi Anthony,

    Actually I received a chem ID value of 7459 , that has to be configured to the fuel gauge. They got the chem ID after analysis. Could you please help me if its even possible to change the value to 7459 ?

    Thanks for your prompt response

  • Hi Aldrina,

    For a chemID outside of the three preprogrammed profiles to be used, one of our flash devices would need to be used. This would not be possible for the bq27426.

    If you send over the report from the GPCCHEM tool, I can take a look into it.

    Regards,

    Anthony Baldino

  • Hi Anthony,

    I configured the golden learning data and also tried to update to a custom chemID. But still the voltage readings that I am getting from the fuel gauge is not quite accurate. I have put the device on charging mode. There is clearly a big offset in the voltage value. What could be the reason.

    And how can I validate all the values that I read from the fuel gauge?

    thanks

  • Hi Aldrina,

    Was the chemID changed after golden learning has been done? This should not be done since it will greatly affect the gauging accuracy.

    Regarding the voltage difference, has there been any calibration completed yet?

    Regards,

    Anthony Baldino

  • Hi Anthony,

    I have configured the correct chemID, but I havent done any calibration yet for difference in voltage.

    Thanks

    Aldrina

  • Hello,

    Today's a holiday and no one is in the office. We will get back to you tomorrow.

    Regards,

    Nick Richards

  • Hi Aldrina,

    For clarification, when you say that the correct chemID has been configured, do you mean one of the three preprogrammed chemIDs for bq27426?

    Can you please tell me how large is the seen offset for the voltage?

    Regards,

    Anthony Baldino

  • Hi Anthony,

    I configured one of the preprogrammed chemIDs. when the USB is plugged in for charging the voltage rises by almost 2-3Volts, than when it is unplugged.

    Thanks

  • Hi Aldrina,

    Are there connections on the schematic between the cell and USB that could cause this rise in voltage?

    If you send the schematic we can take a look into it.

    Regards,

    Anthony Baldino