Whenever the TPS543820 is powered up, and then powered down, the input power pins (Vin) are low impedance (less than 1 ohm). It can take up to 40 minutes before the impedance rises again to high impedance. If you apply power again, the circuit is fine, and there are no shorts.
The issue is with in-circuit testing. Our manufacturing group is trying to get an ICT fixture working to test these parts and are complaining about the low impedance on Vin when they power down which makers their test fail. Can someone explain why we have a low impedance after powering down the device? Is there anything that can be done to accelerate the return to high impedance? Thanks.