This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A16-Q1: spec check

Part Number: TPS7A16-Q1


Hi

Could you help to suggest the parts with tps7A1601Q1 pin to pin, the current requirement is 0.2A ,Thanks

  • Hi Gareth, 

    Thank you for your questions! One p2p drop in alternative would be the TPS7A1601ADGNR

    The best replacements I would suggest are the TLV76701DGNR and TPS7B82-Q1  (fixed versions only), since they would be able to see the 0.2A spec requirement. Neither of these would be drop-in replacements, but they do have the same package with minimal changes need to adjust the layout. 

    Let me know if you have any additional questions. 

    Thanks, 

    McKyla