This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM79L: spec check

Part Number: LM79L


Hi 

Can I confirm with you that when using the LM79L05ACM, if the input power supply is +5V, the output is -5V?

  • Hey Gareth,

    LM79L regulates a negative input voltage to a negative output voltage with a lower absolute value. 

    In the case of LM79L05ACM, your input voltage must be greater than or equal to Output Voltage (-5V) + Dropout Voltage (-1.7V), or between -30V and -6.7V input for this device to properly regulate -5V. 

    BR,

    Erin