This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: USB-C I/O Hub can't light up MSI Optix MAG161V and MSI Optix MAG162V display with TI TPS65987DDH IC

Part Number: TPS65987D
Other Parts Discussed in Thread: TPS55288

attached the USB-C I/O Hub block diagram.

attached the USB-C I/O Hub current F/W *.pjt file. p473_out_if_01_U35 DFP_987D_F7071038_USB3 initial events_20240424_disable support USB Gen2 signalling in 0x51_full.zip

USB-C display list:

Without adapter(output from TPS55288):

ELO, ET1002L => USB-C cable standard plug and reverse plug test OK pass.

ASUS, MB16AC => USB-C cable standard plug and reverse plug test OK pass.

MSI, Optix MAG162V => Fail(always show MSI logo, repeat reboot…)

MSI, Optix MAG161V => Fail(show no signal, then turn off display)

ELO, ET1502L-2UWC-1-G => USB-C cable standard plug and reverse plug test OK pass.

DN, D1150 => USB-C cable standard plug and reverse plug test OK pass.

 

With adapter:

DN, D1150 => USB-C cable standard plug and reverse plug test OK pass.

ViewSonic, VS17552 => USB-C cable standard plug and reverse plug test OK pass.

Please help to check the TPS65987DDH USB-C F/W to light up the MSI Optix MAG161V and MSI Optix MAG162V display.

thanks.