Part Number: TPS7A96
LDO team,
Can you help with explaining a little more about the PG trip point for the TPS7A96? If the Rfb Top and Bottom is set to 187K and 12.4K respectively in order to give a 3.3V output, the resulting Vfb_pg = 0.205V. This is actually lower than the max value for FB_PG pin trip point (rising), which is 0.21V (on page 7 of the datasheet). If 0.21V is really the trip point for PG, then this would be concerning since the voltage may never reach this trip point.
However, my understanding is that the PG pin will go high at 95% of 0.21V, based on the Note on page 29. So PG will be high when Vfb_pg reaches 0.1995V.
Is that correct?
Thanks,
Darren