This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792: Inductor value

Part Number: BQ25792

Hello all,

The BQ25792 requires 1uH typ. inductor (no min/max values) using 1.5MHz switching frequency.

Most common inductors have +/-20% tolerance so actual inductance can go down to 0.8uH at higher currents

Is it ok to use a slightly larger 1.2uH inductor for the BQ25792?

Thanks!

Nir