Hello,
We are using zeners on the cell inputs to the BQ294502, but we're having some issues with open cell detect.
- What is the failure mode if exceed the absolute max for V3 to V2 or V2 to V1.
- This is determine if we need the Zener Diodes protection
- What is the best solution we should implement? Right now we had Zener between each pin but apparently this causing no detection on open cells.
- We have to remove those Zeners for our current build in order to keep open cell and avoid faulting after removing the 3s pack.
- What is the recommended solution from TI in this case?
Thank you, Keith